VBUS.ACNOMINAL

Description

This keyword lets the user easily configure the operating voltage for a level other than the default of the drive.


  • The user can only de-rate a drive, and not operate it higher than the original voltage.

When changed, VBUS.ACNOMINAL will modify the inrush voltage settings as well as the Regen voltage configurations. It is important that VBUS.ACNOMINAL be set as accurately as possible to minimize voltage faults.

Examples

Code

If an HV drive (480V) was needed for bench testing at 120V, the user would do the following

VBUS.ACNOMINAL 120

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

VAC

Range

0 to Drive Rated Voltage

Default Value

Drive Rated Voltage

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen